USB Ports

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Ports

1,518件の閲覧回数
mylsamy_m
Contributor I

Hi,

In iMx6  dual, we noticed we have 4 usb ports( One USB 2.0 OTG and 3 USB2.0 hosts)

but we can able to see the pin out only for one USB 2.0 OTG and One HOST.

I hope if we need two more host do I need to drive through USB HUB or how can I do that?

Thanks and Regards

ラベル(1)
0 件の賞賛
返信
1 返信

1,449件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

The pinout availability will depend of the used board. In case of requiring more Host ports and you only have one, you may use an external HUB (just considering power requirements).

For additional details regarding USB controllers and configuration, you could take a look to application note AN4589 “Configuring USB on i.MX 6 Series Processors”.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 件の賞賛
返信