USB Ports

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Ports

1,516 Views
mylsamy_m
Contributor I

Hi,

In iMx6  dual, we noticed we have 4 usb ports( One USB 2.0 OTG and 3 USB2.0 hosts)

but we can able to see the pin out only for one USB 2.0 OTG and One HOST.

I hope if we need two more host do I need to drive through USB HUB or how can I do that?

Thanks and Regards

Labels (1)
0 Kudos
Reply
1 Reply

1,447 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

The pinout availability will depend of the used board. In case of requiring more Host ports and you only have one, you may use an external HUB (just considering power requirements).

For additional details regarding USB controllers and configuration, you could take a look to application note AN4589 “Configuring USB on i.MX 6 Series Processors”.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos
Reply