USB Overcurrent Detection process for MX6Q-SABRE-SD with AndroidKK4.4.3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB Overcurrent Detection process for MX6Q-SABRE-SD with AndroidKK4.4.3

2,959 次查看
yuuki
Senior Contributor II

Dear all,

We evaluate AndroidKK4.4.3 on SABRE-SDB.

When Overcurrent is detected on a USB port, what kind of processing is executed?

May I have advice?

Best Regards,
Yuuki

标签 (2)
0 项奖励
回复
1 回复

1,930 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

if "disable-over-current" is enabled in dtsi file

linux/imx6qdl-sabresd.dtsi at master · torvalds/linux · GitHub

USB module performs processing described in sect.

65.4.3.2.5 Port Reporting Over-Current and Table 65-37

i.MX6DQ Reference Manual (rev.3  7/2015)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Details of driver behaviour one can find looking at usb driver sources

in attached Linux Manual Table 41-1 USB Driver Files.

On SABRE-SDB MIC2026 (U515 in sabre schematic spf-27392.pdf) limits current at

overcurrent condition.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复