USB Mass Storage drivers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Mass Storage drivers

3,087 Views
saida
Contributor II

Hi
Can any one have USB mass storage drivers for i.mx6 board (baremetal)

please help me in this regard

 

 

Labels (1)
0 Kudos
Reply
4 Replies

2,410 Views
saida
Contributor II

HI every one
i have customized board based on i.mx6 dual lite
i am developing a bare metal USB ,ass storage protocol
Enumeration done successfully for my pen drive
base of Enumeration code taken from SDK and modified for MSD
SCSI protocol related code taken from u-boot
it has COMMAND PHASE, DATA PHASE and STATUS PHASE
i am not controlling port power through GPIO, instead connected directly to POWER
COMMAND PAHSE transaction processed successfully
DATA PHASE, i am getting token=0x01F38D08
when i refer reference manual, it is transaction error
what could be the issue
can any one help in this regard
i am struggling lot
if required i shared the code
thanks and regards

Saida

Tags (1)
0 Kudos
Reply

3,068 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

It can support USB mass storage, what problem have you met, it maybe cause by the hardware problem.

0 Kudos
Reply

2,394 Views
saida
Contributor II
hi
can you check my post regarding usb Bulk transfer
0 Kudos
Reply

3,059 Views
saida
Contributor II

I want source code for USB Mass storage device

SDK do not have example for mass storage, it has only key board and mouse examples

Regards

Saida

0 Kudos
Reply