USB 3 Polarity Inversion TX and RX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB 3 Polarity Inversion TX and RX

跳至解决方案
6,115 次查看
MNTR
Contributor I

Hello,

according to the USB3 spec it is allowed to invert the polarity of the USB_TX or USB_RX signals without any further adjustments.

Since we got some issues with our USB-Interface where we inverted USB2_TX_N and USB2_TX_P as well as USB2_RX_N and USB2_RX_P, I want to make sure this is allowed with the i.MX8M Plus.

Can anybody confirm this inversion is possible and we do not have to adjust any settings or similar?

IMX8MPLUS 

0 项奖励
回复
1 解答
6,089 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @MNTR,

I hope you are doing well.

TX/RX polarity inversion is supported on i.MX8MP.

USB 3.0 PHY has auto polarity detection and adjustment support.

Thanks & Regards,
Dhruvit Vasavada

 

在原帖中查看解决方案

3 回复数
6,073 次查看
MNTR
Contributor I

Hi @Dhruvit ,

thank you very much. 
Are there any limitations? 
For example: can I invert just one of the super speed pairs (TX inverted, RX not inverted)? 

Thanks in advance

0 项奖励
回复
6,024 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @MNTR,

I hope you are doing well.

i.MX8MP has Synopsys USB 3.0 PHY.

Lane Polarity inversion only talks about Rx signals.

Please refer to Universal Serial Bus 3.0 Specification for more information.

Thanks & Regards,
Dhruvit Vasavada

6,090 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @MNTR,

I hope you are doing well.

TX/RX polarity inversion is supported on i.MX8MP.

USB 3.0 PHY has auto polarity detection and adjustment support.

Thanks & Regards,
Dhruvit Vasavada