USB 3 Polarity Inversion TX and RX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB 3 Polarity Inversion TX and RX

ソリューションへジャンプ
6,077件の閲覧回数
MNTR
Contributor I

Hello,

according to the USB3 spec it is allowed to invert the polarity of the USB_TX or USB_RX signals without any further adjustments.

Since we got some issues with our USB-Interface where we inverted USB2_TX_N and USB2_TX_P as well as USB2_RX_N and USB2_RX_P, I want to make sure this is allowed with the i.MX8M Plus.

Can anybody confirm this inversion is possible and we do not have to adjust any settings or similar?

IMX8MPLUS 

0 件の賞賛
返信
1 解決策
6,051件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @MNTR,

I hope you are doing well.

TX/RX polarity inversion is supported on i.MX8MP.

USB 3.0 PHY has auto polarity detection and adjustment support.

Thanks & Regards,
Dhruvit Vasavada

 

元の投稿で解決策を見る

3 返答(返信)
6,035件の閲覧回数
MNTR
Contributor I

Hi @Dhruvit ,

thank you very much. 
Are there any limitations? 
For example: can I invert just one of the super speed pairs (TX inverted, RX not inverted)? 

Thanks in advance

0 件の賞賛
返信
5,986件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @MNTR,

I hope you are doing well.

i.MX8MP has Synopsys USB 3.0 PHY.

Lane Polarity inversion only talks about Rx signals.

Please refer to Universal Serial Bus 3.0 Specification for more information.

Thanks & Regards,
Dhruvit Vasavada

6,052件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @MNTR,

I hope you are doing well.

TX/RX polarity inversion is supported on i.MX8MP.

USB 3.0 PHY has auto polarity detection and adjustment support.

Thanks & Regards,
Dhruvit Vasavada