UDP/RTP streaming orders of gstreamer decoder/encoder

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UDP/RTP streaming orders of gstreamer decoder/encoder

2,550 Views
tutran
Contributor I

Hi there,

When I read the tutorial of Yocto/Gstreamer

Yocto/gstreamer/streaming – Gateworks

I saw that the example pipeline for UDP/RTP(raw) always start with decoder part first, then start encoder.

I wonder if there is any specific reason for this, can anybody help me to explain it?

In my practical test with iMX6DL board and streaming from camera, also I have the same result. If starting decoder from client side first, then start streaming from iMX6, I can see the video perfectly. In opposite case, it does not work though two streaming pipeline still is running, but I cannot see the decoded video displayed on Ubuntu client PC

Labels (2)
0 Kudos
Reply
2 Replies

2,337 Views
tutran
Contributor I

Dear Artur,

Thanks for your reply. I just ask because I saw some pipelines from gstreamer that guide us to start pipeline from server, then copy the caps properties to the client side. It also works

0 Kudos
Reply

2,337 Views
art
NXP Employee
NXP Employee

Of course, the receiving part should start first to wait for the incoming stream and then handle and decode the stream header correctly. In other case, the receiving part will not be able to synchronize with the stream.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply