Hey there.
We are trying to configure UART1 in DTE mode as our product will mainly interface with modems and other DCE hardware.
When configuring UART1 to DCE mode in the device tree, data gets sent out of the correct pin and gets correctly received after connecting RX and TX straight through.
But when UART1 is configured to DTE mode, the data gets sent out of the RX pin. So far so good. DTE mode seems to work.
But when trying to read the content of UART1 in the console by the help of "cat /dev/ttymxc0", no data is displayed. When executing the same command in DCE mode, the sent data is displayed.
Our device tree is pasted below. The commented parts are for UART1 in DCE mode. No hardware handshake is used ATM. Also attached is the latest bootlog of the system. I have also tried to configure UART3 into DTE mode which works without a problem. The sent out data is received and shown in the console.
Am I missing something with the configuration of UART1?
// SPDX-License-Identifier: (GPL-2.0+ OR MIT)
/*
* Copyright 2019 NXP
* Copyright 2019-2021 Variscite Ltd.
*/
#include "imx8mm-var-som-embcustom.dtsi"
/ {
model = "Variscite VAR-SOM-MX8M-MINI on a.Box FSD rev2021";
chosen {
bootargs = "console=ttymxc3,115200 earlycon=ec_imx6q,0x30a60000,115200";
bootargs-append = "console=ttymxc3,115200 earlycon=ec_imx6q,0x30a60000,115200 androidboot.console=ttymxc3 androidboot.primary_display=imx-drm androidboot.board=varsommx8mmini androidboot.bt_uart=/dev/ttymxc1 androidboot.bt_sdio=/sys/bus/mmc/devices/mmc0:0001/mmc0:0001:1/device androidboot.bt_firmware=BCM43430A1.hcd androidboot.bt_sdio_id=0xa9a6 androidboot.wificountrycode=CN";
stdout-path = &uart4;
};
backlight: backlight {
compatible = "pwm-backlight";
pwms = <&pwm1 0 1000000 0>;
brightness-levels = < 0 1 2 3 4 5 6 7 8 9
10 11 12 13 14 15 16 17 18 19
20 21 22 23 24 25 26 27 28 29
30 31 32 33 34 35 36 37 38 39
40 41 42 43 44 45 46 47 48 49
50 51 52 53 54 55 56 57 58 59
60 61 62 63 64 65 66 67 68 69
70 71 72 73 74 75 76 77 78 79
80 81 82 83 84 85 86 87 88 89
90 91 92 93 94 95 96 97 98 99
100>;
default-brightness-level = <80>;
status = "okay";
};
gpio-keys {
compatible = "gpio-keys";
status = "okay";
wakeup {
label = "Wakeup";
gpios = <&gpio1 14 GPIO_ACTIVE_HIGH>;
linux,code = <143>;
wakeup-source;
};
};
};
&i2c3 {
/* Capacitive touch controller */
/* ft5x06_ts: ft5x06_ts@38 {
compatible = "edt,edt-ft5206";
reg = <0x38>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_captouch>;
interrupt-parent = <&gpio5>;
interrupts = <4 IRQ_TYPE_EDGE_FALLING>;
touchscreen-size-x = <800>;
touchscreen-size-y = <480>;
touchscreen-inverted-x;
touchscreen-inverted-y;
wakeup-source;
status = "okay";
};
*/
/* DS1337 RTC module */
rtc@68 {
compatible = "dallas,ds1337";
reg = <0x68>;
status = "okay";
};
};
/*
&mipi_csi_1 {
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
port {
mipi1_sensor_ep: endpoint@1 {
remote-endpoint = <&ov5640_mipi1_ep>;
data-lanes = <2>;
csis-hs-settle = <13>;
csis-clk-settle = <2>;
csis-wclk;
};
csi1_mipi_ep: endpoint@2 {
remote-endpoint = <&csi1_ep>;
};
};
};
&csi1_bridge {
fsl,mipi-mode;
status = "okay";
port {
csi1_ep: endpoint {
remote-endpoint = <&csi1_mipi_ep>;
};
};
};
*/
&pwm1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_pwm1>;
status = "okay";
};
&pwm2 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_pwm2>;
};
/* Full Serial UART, LSA Modems e.g. */
&uart1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_uart1>;
fsl,dte-mode;
/* fsl,uart-has-rtscts; */
status = "okay";
};
/* IBIS UART */
&uart3 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_uart3>;
status = "okay";
};
/* Console via FTDI Converter */
&uart4 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_uart4>;
/delete-property/ dmas;
/delete-property/ dma-names;
status = "okay";
};
&usbotg1 {
dr_mode = "peripheral";
picophy,pre-emp-curr-control = <3>;
picophy,dc-vol-level-adjust = <7>;
srp-disable;
hnp-disable;
adp-disable;
/* extcon = <0>, <&extcon_usb1>; */
status = "okay";
};
&usbotg2 {
dr_mode = "host";
/* vbus-supply = <®_usb_otg2_vbus>; */
picophy,pre-emp-curr-control = <3>;
picophy,dc-vol-level-adjust = <7>;
disable-over-current;
status = "okay";
};
/* SD */
/*
&usdhc2 {
pinctrl-names = "default", "state_100mhz", "state_200mhz";
pinctrl-0 = <&pinctrl_usdhc2>, <&pinctrl_usdhc2_gpio>;
pinctrl-1 = <&pinctrl_usdhc2_100mhz>, <&pinctrl_usdhc2_gpio>;
pinctrl-2 = <&pinctrl_usdhc2_200mhz>, <&pinctrl_usdhc2_gpio>;
cd-gpios = <&gpio1 10 GPIO_ACTIVE_LOW>;
bus-width = <4>;
vmmc-supply = <®_usdhc2_vmmc>;
status = "okay";
};
*/
&gpio1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_gpio1>;
status = "okay";
};
&gpio2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_gpio2>;
status = "okay";
};
&gpio4 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_gpio4>;
status = "okay";
};
&gpio5 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_gpio5>;
status = "okay";
};
/*
&snvs_pwrkey {
status = "okay";
};
&snvs_rtc {
status = "disabled";
};
*/
&iomuxc {
pinctrl_pwm1: pwm1grp {
fsl,pins = <
MX8MM_IOMUXC_SPDIF_EXT_CLK_PWM1_OUT 0x06
>;
};
pinctrl_pwm2: pwm2grp {
fsl,pins = <
MX8MM_IOMUXC_SPDIF_RX_PWM2_OUT 0x06
>;
};
pinctrl_uart1: uart1grp {
fsl,pins = <
MX8MM_IOMUXC_UART1_RXD_UART1_DTE_TX 0x140
MX8MM_IOMUXC_UART1_TXD_UART1_DTE_RX 0x140
MX8MM_IOMUXC_SAI2_RXD0_UART1_DTE_CTS_B 0x140
MX8MM_IOMUXC_SAI2_TXFS_UART1_DTE_RTS_B 0x140
>;
};
/* pinctrl_uart1: uart1grp { */
/* fsl,pins = < */
/* MX8MM_IOMUXC_UART1_RXD_UART1_DCE_RX 0x140 */
/* MX8MM_IOMUXC_UART1_TXD_UART1_DCE_TX 0x140 */
/* MX8MM_IOMUXC_SAI2_RXD0_UART1_DCE_RTS_B 0x140 */
/* MX8MM_IOMUXC_SAI2_TXFS_UART1_DCE_CTS_B 0x140 */
/* >; */
/* }; */
pinctrl_uart3: uart3grp {
fsl,pins = <
MX8MM_IOMUXC_UART3_RXD_UART3_DCE_RX 0x140
MX8MM_IOMUXC_UART3_TXD_UART3_DCE_TX 0x140
>;
};
pinctrl_uart4: uart4grp {
fsl,pins = <
MX8MM_IOMUXC_UART4_RXD_UART4_DCE_RX 0x140
MX8MM_IOMUXC_UART4_TXD_UART4_DCE_TX 0x140
>;
};
pinctrl_gpio1: gpio1grp {
fsl,pins = <
MX8MM_IOMUXC_GPIO1_IO01_GPIO1_IO1 0x16 /*DISP_BL_W_SHDN*/
MX8MM_IOMUXC_GPIO1_IO03_GPIO1_IO3 0x16 /*DISP_BL_G_SHDN*/
MX8MM_IOMUXC_GPIO1_IO06_GPIO1_IO6 0x16 /*SOM_Alive*/
MX8MM_IOMUXC_GPIO1_IO08_GPIO1_IO8 0x16 /*var_DC_EN*/
MX8MM_IOMUXC_GPIO1_IO10_GPIO1_IO10 0x16 /*DO1_EN*/
MX8MM_IOMUXC_GPIO1_IO11_GPIO1_IO11 0x16 /*LED 0*/
MX8MM_IOMUXC_GPIO1_IO12_GPIO1_IO12 0x16 /*I_IGN*/
MX8MM_IOMUXC_GPIO1_IO13_GPIO1_IO13 0x16 /*24V_1A_2_EN*/
MX8MM_IOMUXC_GPIO1_IO14_GPIO1_IO14 0x16 /*Wake pin from watchdog*/
>;
};
pinctrl_gpio2: gpio2grp {
fsl,pins = <
MX8MM_IOMUXC_SD2_CLK_GPIO2_IO13 0x16 /*I_Signal_2*/
MX8MM_IOMUXC_SD2_DATA0_GPIO2_IO15 0x16 /*I_Signal_4*/
MX8MM_IOMUXC_SD2_DATA1_GPIO2_IO16 0x16 /*I_Signal_3*/
MX8MM_IOMUXC_SD2_DATA2_GPIO2_IO17 0x16 /*I_Signal_1*/
MX8MM_IOMUXC_SD2_DATA3_GPIO2_IO18 0x16 /*I_Signal_C4*/
MX8MM_IOMUXC_SD2_RESET_B_GPIO2_IO19 0x16 /*SHDN_2V5*/
>;
};
pinctrl_gpio4: gpio4grp {
fsl,pins = <
MX8MM_IOMUXC_SAI1_TXFS_GPIO4_IO10 0x16 /*OPT_OUT_1_EN*/
MX8MM_IOMUXC_SAI1_TXC_GPIO4_IO11 0x16 /*varDC_SHDN*/
MX8MM_IOMUXC_SAI2_RXFS_GPIO4_IO21 0x16 /*DISP_DATA_COM*/
MX8MM_IOMUXC_SAI2_RXC_GPIO4_IO22 0x16 /*SHDN_1V2*/
MX8MM_IOMUXC_SAI2_TXC_GPIO4_IO25 0x16 /*ETH_SW_RST*/
MX8MM_IOMUXC_SAI2_TXD0_GPIO4_IO26 0x16 /*24V_3A_EN*/
MX8MM_IOMUXC_SAI2_MCLK_GPIO4_IO27 0x16 /*KSZ8091_RST*/
MX8MM_IOMUXC_SAI3_RXFS_GPIO4_IO28 0x16 /*BB_SHDN*/
>;
};
pinctrl_gpio5: gpio5grp {
fsl,pins = <
MX8MM_IOMUXC_SAI3_TXD_GPIO5_IO1 0x16 /*DO2_EN*/
MX8MM_IOMUXC_SAI3_MCLK_GPIO5_IO2 0x16 /*5V_EN*/
MX8MM_IOMUXC_ECSPI2_SCLK_GPIO5_IO10 0x16 /*LED 1*/
MX8MM_IOMUXC_ECSPI2_MOSI_GPIO5_IO11 0x16 /*24V_1A_1_EN*/
MX8MM_IOMUXC_ECSPI2_MISO_GPIO5_IO12 0x16 /*OPT_IN*/
MX8MM_IOMUXC_ECSPI2_SS0_GPIO5_IO13 0x16 /*OPT_OUT_2_EN*/
MX8MM_IOMUXC_I2C2_SCL_GPIO5_IO16 0x16 /*USB_HUB_RST*/
MX8MM_IOMUXC_I2C2_SDA_GPIO5_IO17 0x16 /*LAN9513_RST*/
MX8MM_IOMUXC_I2C4_SCL_GPIO5_IO20 0x16 /*DISP_BL_R_SHDN*/
MX8MM_IOMUXC_I2C4_SDA_GPIO5_IO21 0x16 /*CAN_STBY*/
>;
};
};