UART pins condition during power on reset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

UART pins condition during power on reset

跳至解决方案
2,463 次查看
YusukeHirai
Contributor I

Hi,

I am trying to use two CPUs and let them communicate with UART.
(One is MCIMX6Y2CVM08AB, and the other is other manufacturers.)

I was worried about whether both signals were output for the power-on reset condition .

It was confirmed that the cpu of other manufacturers became hi-z and there was no problem.
But I didn't understand the operation of IMX6.
So I have a question about this.

There is a description out of reset condition in the IMX6's data sheet.
However, there is no description of reset condition.
Does anyone know?

The IMX6 uses the following pins
GPIO3_IO0 (LCD_CLK)
GPIO_IO1 (LCD_ENABLE)

Please let me know if anyone knows.


Regards,

Yusuke

 

0 项奖励
回复
1 解答
2,438 次查看
Yuri
NXP Employee
NXP Employee

@YusukeHirai 
Hello,

   During power up sequence and short period of stabilization, also during reset,
i.MX 6ULL pin states
are not pre-defined.

Regards,
Yuri.

 

在原帖中查看解决方案

0 项奖励
回复
7 回复数
2,439 次查看
Yuri
NXP Employee
NXP Employee

@YusukeHirai 
Hello,

   During power up sequence and short period of stabilization, also during reset,
i.MX 6ULL pin states
are not pre-defined.

Regards,
Yuri.

 

0 项奖励
回复
2,426 次查看
ban45
Contributor III

Hello

 

If the connected device is an output, will it conflict?

Is it high impedance during reset?

best regard

0 项奖励
回复
2,409 次查看
Yuri
NXP Employee
NXP Employee

@ban45 
Hello,

  During power on sequence and reset - conflicts are possible.

Regards,
Yuri.

0 项奖励
回复
2,403 次查看
ban45
Contributor III

Hello,

What should I do if I connect another CPU via UART communication?

Other companies' CPUs have high impedance or input during reset.(At power-on reset)

Is there any output during the reset?
In that case, you will break the device that is OUTPUT in the connected device.
Could you please tell me how to connect the output pin to the GPIO pin?

 

best regard

0 项奖励
回复
2,395 次查看
Yuri
NXP Employee
NXP Employee

@ban45 

  Reliable solution - using buffers.

 

~Yuri.

0 项奖励
回复
2,391 次查看
ban45
Contributor III

Hello

Is it the same for memory related such as DDR3?

Is it necessary to buffer everything if the other party is output?

best regard

0 项奖励
回复
2,376 次查看
Yuri
NXP Employee
NXP Employee

@ban45 
Hello,

  Follow i.MX 6ULL reference design - at least - it has been tested.

  Also, from section 4.2.3 (Power Supplies Usage) of i.MX 6ULL Datasheet for Consumer Products
( Rev. 1.3, 08/2018):
  All I/O pins should not be externally driven while the I/O power supply for the pin (NVCC_xxx) is OFF.

Regards,
Yuri.

0 项奖励
回复