UART CTS/RTS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART CTS/RTS

6,288 Views
deepanrajanbara
Contributor IV

Hi Sir,

Ours is Custom board based on imx6 and we required to check the UART flow control for our board.But we are not sure how to check the flow control for imx6 UART.Can anyone please help me in checking the UART flow control(CTS/RTS) in software Kernel level.

Thank you,

Deepanraj.A

6 Replies

4,577 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply

4,577 Views
deepanrajanbara
Contributor IV

Hi

Actually i wanted to check it applications wise is there any application in Linux to check Hardware flow control.

Thank you,

Deepanraj.A

0 Kudos
Reply

4,577 Views
saurabh206
Senior Contributor III

Hi,

You can use mxc_uart_test.

Thanks

Saurabh

0 Kudos
Reply

4,577 Views
JithCR
Contributor III

Hi Saurabh,

May I know how we can test the CTS/RTS using mxc_uart_test.(A high level information)

0 Kudos
Reply

4,577 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jith

please look at attached doc file from

imx-test-3.0.35-4.1.0.

~igor

0 Kudos
Reply

4,577 Views
saurabh206
Senior Contributor III
0 Kudos
Reply