UART CTS/RTS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART CTS/RTS

6,263件の閲覧回数
deepanrajanbara
Contributor IV

Hi Sir,

Ours is Custom board based on imx6 and we required to check the UART flow control for our board.But we are not sure how to check the flow control for imx6 UART.Can anyone please help me in checking the UART flow control(CTS/RTS) in software Kernel level.

Thank you,

Deepanraj.A

ラベル(7)
6 返答(返信)

4,552件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信

4,552件の閲覧回数
deepanrajanbara
Contributor IV

Hi

Actually i wanted to check it applications wise is there any application in Linux to check Hardware flow control.

Thank you,

Deepanraj.A

0 件の賞賛
返信

4,552件の閲覧回数
saurabh206
Senior Contributor III

Hi,

You can use mxc_uart_test.

Thanks

Saurabh

0 件の賞賛
返信

4,552件の閲覧回数
JithCR
Contributor III

Hi Saurabh,

May I know how we can test the CTS/RTS using mxc_uart_test.(A high level information)

0 件の賞賛
返信

4,552件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jith

please look at attached doc file from

imx-test-3.0.35-4.1.0.

~igor

0 件の賞賛
返信

4,552件の閲覧回数
saurabh206
Senior Contributor III
0 件の賞賛
返信