UAF of AMediaFormat in Android Automotive

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

UAF of AMediaFormat in Android Automotive

510 次查看
dmitry_sidorenkov
Contributor III

Using NXP Android automotive 12.1 found an UAF.
I could not find out a github to create a PR or NXP's Android bugs forum.

soc: imx8qm
linux: 5.15.52

Root cause:
AMediaFormat_delete(extractor_meta) deletes a String8 field of extractor_meta, then it is implicitly used in strcasecmp via containerMime at the next line.

Fix:
Move deleting below then strcasecmp

 

--- a/extractor/ImxExtractor.cpp
+++ b/extractor/ImxExtractor.cpp
@@ -111,10 +111,10 @@ ImxMediaSource::ImxMediaSource(ImxExtractor *extractor, size_t index, AMediaForm
     if(AMEDIA_OK == mExtractor->getMetaData(extractor_meta)){
         AMediaFormat_getString(extractor_meta, AMEDIAFORMAT_KEY_MIME, &containerMime);
     }
-    AMediaFormat_delete(extractor_meta);
 
     mIsVorbis = containerMime != NULL && !strcasecmp(containerMime, MEDIA_MIMETYPE_CONTAINER_MATROSKA) && !strcasecmp(mime, MEDIA_MIMETYPE_AUDIO_VORBIS);
     mIsMP4 = containerMime != NULL && !strcasecmp(containerMime, MEDIA_MIMETYPE_CONTAINER_MPEG4);
+    AMediaFormat_delete(extractor_meta);
 
     mNALLengthSize = 0;
     mBufferSize = 0;

 

标签 (1)
0 项奖励
回复
0 回复数