UAF of AMediaFormat in Android Automotive

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UAF of AMediaFormat in Android Automotive

506件の閲覧回数
dmitry_sidorenkov
Contributor III

Using NXP Android automotive 12.1 found an UAF.
I could not find out a github to create a PR or NXP's Android bugs forum.

soc: imx8qm
linux: 5.15.52

Root cause:
AMediaFormat_delete(extractor_meta) deletes a String8 field of extractor_meta, then it is implicitly used in strcasecmp via containerMime at the next line.

Fix:
Move deleting below then strcasecmp

 

--- a/extractor/ImxExtractor.cpp
+++ b/extractor/ImxExtractor.cpp
@@ -111,10 +111,10 @@ ImxMediaSource::ImxMediaSource(ImxExtractor *extractor, size_t index, AMediaForm
     if(AMEDIA_OK == mExtractor->getMetaData(extractor_meta)){
         AMediaFormat_getString(extractor_meta, AMEDIAFORMAT_KEY_MIME, &containerMime);
     }
-    AMediaFormat_delete(extractor_meta);
 
     mIsVorbis = containerMime != NULL && !strcasecmp(containerMime, MEDIA_MIMETYPE_CONTAINER_MATROSKA) && !strcasecmp(mime, MEDIA_MIMETYPE_AUDIO_VORBIS);
     mIsMP4 = containerMime != NULL && !strcasecmp(containerMime, MEDIA_MIMETYPE_CONTAINER_MPEG4);
+    AMediaFormat_delete(extractor_meta);
 
     mNALLengthSize = 0;
     mBufferSize = 0;

 

ラベル(1)
0 件の賞賛
返信
0 返答(返信)