U-boot Hang at Authenticate Image from DDR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

U-boot Hang at Authenticate Image from DDR

跳至解决方案
2,077 次查看
trongthinh
Contributor IV

I am using u-boot 2016.03 on iMX6Dual (meta-freescale, branch pyro). I followed 2 documents (IMX Application trust Architecture, High assurance Boot Hab dummy) to enable secure boot and sign u-boot/kernel. 

=> load mmc 1 12800000 zImage

And

=> hab_auth_img 12800000 600000

U-boot hangs here. Bellow is the log:

U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+g48ab39e06f (Dec 13 2018 - 10:18:45 +0700)

CPU: Freescale i.MX6D rev1.5 at 792MHz
CPU: Industrial temperature grade (-40C to 105C) at 43C
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x10
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1 is current device
Use ethernet address from eMMC d2:83:38:6d:af:37.
Net: Board Net Initialization Failed
No ethernet found.
Normal Boot
Hit any key to stop autoboot: 0
=> load mmc 1 12800000 zImage
reading zImage
6297944 bytes read in 307 ms (19.6 MiB/s)
=> hab_auth_img 12800000 600000

Authenticate image from DDR location 0x12800000...

My question is "What is the possible cause?" Is there any suggestion?

标签 (2)
标记 (3)
1 解答
1,886 次查看
trongthinh
Contributor IV

Hi Yuri,

The problem is script genIVT has some fixed values (Jump location, Self Pointer, CSF pointer). I did not change these values to the correct one for my kernel. I solved the problem by changing these values. Here is a script var-genIVT of someone on GitHub that helps me do the job faster.

Thank for your help!

在原帖中查看解决方案

2 回复数
1,886 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   Please try to get HAB log, using JTAG to read data from 0x00904000, size 0x0B80.  


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,887 次查看
trongthinh
Contributor IV

Hi Yuri,

The problem is script genIVT has some fixed values (Jump location, Self Pointer, CSF pointer). I did not change these values to the correct one for my kernel. I solved the problem by changing these values. Here is a script var-genIVT of someone on GitHub that helps me do the job faster.

Thank for your help!