U-Boot initializing failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-Boot initializing failure

1,648件の閲覧回数
JosSchuts
Contributor I

For a week or so I work with the i.MX53 QSB. In this time I've managed to start up both a Linux Gnome build and Windows Compact 7 on the QSB via uSD. Only today I've failed to start up the Linux builds of the FSL orginal uSD with Ubuntu as well as my own Linux Gnome build. 

When I try to start up Linux, the QSB won't give any output to the serial console and won't start the start-up sequence. However, when I try to start up Windows Compact 7, all works fine.

Because I get no serial feedback from the QSB, I think it's safe to assume that the problem is caused by U-boot..? Or is there anything else I should know about the prebootloader that can cause this problem.

Please, can anyone help with finding the problem?

ラベル(1)
0 件の賞賛
返信
1 返信

1,608件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

Where is the prebootloader for WINCE boot placed?

0 件の賞賛
返信