imx53 QSB boots but stuck in the penguin log screen (VGA)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx53 QSB boots but stuck in the penguin log screen (VGA)

2,772 Views
KonstantinosTsi
Contributor I

Hi all,

 

I successfully loaded the appropriate files in a 4GB SD card.

However when the board boots from this new SD card it is getting stuck in the black screen with the linux penguin logo in the upper left corner.

The last messages in the debug are:

 

VFS: Mounted root (ext3 filesystem) on device 179:1.                           
Freeing init memory: 172K                                                      
init started: BusyBox v1.15.0 ()                                               
starting pid 1176, tty '': '/etc/rc.d/rcS'                                     
Mounting /proc and /sys                                                        
Starting the hotplug events dispatcher udevd                                   
Synthesizing initial hotplug events                                            
Setting the hostname to freescale                                              
Mounting filesystems                                                           
cp: write error: No space left on device                                       
mount: mounting usbfs on /proc/bus/usb failed: No such file or directory       
Starting inetd:                                                                
starting pid 2207, tty '': '/sbin/getty -L ttymxc0 115200 vt100                
arm-none-linux-gnueabi-gcc (4.4.4_09.06.2010) 4.4.4                            
root filesystem built on Thu, 24 Nov 2011 17:28:13 -0600                       
Freescale Semiconductor, Inc.                                                                                                                                  
freescale login:

by typing root i can see the root file system and everything but nothing in the VGA screen.

I will appreciate any opinion/solution

 

Kostas

Tags (1)
0 Kudos
Reply
5 Replies

2,645 Views
KonstantinosTsi
Contributor I

just with the username:root is ok,

doesn.t want password

0 Kudos
Reply

2,645 Views
Venku
Contributor I

What is the default username and password?

0 Kudos
Reply

2,645 Views
VladanJovanovic
NXP Employee
NXP Employee

What do you mean with complete compilation?

0 Kudos
Reply

2,645 Views
KonstantinosTsi
Contributor I

ok

I thought that it will be a complete compilation.

Is there a documentation for that?

Thanks for the reply

0 Kudos
Reply

2,645 Views
VladanJovanovic
NXP Employee
NXP Employee

Sounds good. What did you expect to see on the screen? :-)

 

Default build with LTIB will produce only that on the screen. Now it's up to you to configure the system to start some graphical app (X with some window manager, or GNOME mobile or something else)...

0 Kudos
Reply