Two camera simultaneously streaming support processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Two camera simultaneously streaming support processor

2,546件の閲覧回数
vidyasagar
Contributor III

Hi All,

Could any one please suggest me which microprocessor support two camera streaming simultaneously.

Our project requirement, should support 2 camera streaming simultaneously and 4 fps, should have 20-40 msec latency with Linux file system.

Please suggest me processor module and how will get technical support from freescale for all technical things.

Thanks,

Vidya

タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,145件の閲覧回数
mohammedazlum
Contributor IV

Hi Vidya


iMX6Q will be supported.

Regards,

Azlum

0 件の賞賛
返信

2,145件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vidya

i.MX6 can do this job, streaming is discussed widely on Community as

on link below.

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale

GStreamer i.MX6 Camera Streaming

Regarding guaranteed latency - this is not simple task, since in general linux

is not real time system. If you wish that Freescale did all technical support for

you can apply to Freescale Professional Services to develop it.

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_PROFESSIONAL

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信