Two camera input on i.MX RT1170

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Two camera input on i.MX RT1170

跳至解决方案
1,918 次查看
scarletlee
Contributor III

Hi,

I want to show 2 camera view on panel same time. The concept as below :

image.png

And I found the this picture as below :

image.png

So...maybe i.MX RT1170 can't support 2 camera input as same time? Or it is possible but MCU must high speed switch VIDEO_MUX?

标签 (1)
0 项奖励
回复
1 解答
1,909 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @scarletlee ,

   Your understanding is correct!

   When you use two camera, even one connect to MIPI-CSI, another connect to the parallel CSI module, you still can't work it at the same time. As you see,  MIPI-CSI and parrallel CSI at last connect to the CSI module, so you can't make the two camea input at the same time.

   So, another solution is use the flexIO connect the second camera.

  You can refer to this post:

https://www.nxp.com/docs/en/application-note/AN12686.pdf

 

Wish it helps you!

If you still have questions about it, please kindly let me know.

Best Regards,

Kerry

在原帖中查看解决方案

1 回复
1,910 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @scarletlee ,

   Your understanding is correct!

   When you use two camera, even one connect to MIPI-CSI, another connect to the parallel CSI module, you still can't work it at the same time. As you see,  MIPI-CSI and parrallel CSI at last connect to the CSI module, so you can't make the two camea input at the same time.

   So, another solution is use the flexIO connect the second camera.

  You can refer to this post:

https://www.nxp.com/docs/en/application-note/AN12686.pdf

 

Wish it helps you!

If you still have questions about it, please kindly let me know.

Best Regards,

Kerry