Two camera input on i.MX RT1170

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Two camera input on i.MX RT1170

Jump to solution
2,501 Views
scarletlee
Contributor III

Hi,

I want to show 2 camera view on panel same time. The concept as below :

image.png

And I found the this picture as below :

image.png

So...maybe i.MX RT1170 can't support 2 camera input as same time? Or it is possible but MCU must high speed switch VIDEO_MUX?

Labels (1)
0 Kudos
Reply
1 Solution
2,492 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @scarletlee ,

   Your understanding is correct!

   When you use two camera, even one connect to MIPI-CSI, another connect to the parallel CSI module, you still can't work it at the same time. As you see,  MIPI-CSI and parrallel CSI at last connect to the CSI module, so you can't make the two camea input at the same time.

   So, another solution is use the flexIO connect the second camera.

  You can refer to this post:

https://www.nxp.com/docs/en/application-note/AN12686.pdf

 

Wish it helps you!

If you still have questions about it, please kindly let me know.

Best Regards,

Kerry

View solution in original post

1 Reply
2,493 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @scarletlee ,

   Your understanding is correct!

   When you use two camera, even one connect to MIPI-CSI, another connect to the parallel CSI module, you still can't work it at the same time. As you see,  MIPI-CSI and parrallel CSI at last connect to the CSI module, so you can't make the two camea input at the same time.

   So, another solution is use the flexIO connect the second camera.

  You can refer to this post:

https://www.nxp.com/docs/en/application-note/AN12686.pdf

 

Wish it helps you!

If you still have questions about it, please kindly let me know.

Best Regards,

Kerry