Trying to enbale UART CTS and RTS flow control not working on imx93

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Trying to enbale UART CTS and RTS flow control not working on imx93

752 次查看
arun_mozhi_thevan
Contributor I

Use two NXP-IMX93 custom board and use dupont cable connect to each other , DUT 's UART_B_TX (Pin5) to Server's UART_B_RX (Pin6) , DUT 's  UART_B_RTS# (Pin7) to  Server's UART_B_CTS# (Pin8)



open minicom on DUT board with hardware flow control enbaled and echo "ABCD" > /dev/ttyLP6 on another server module , but we could not able to get data 

while trying to send data from DUT to server through UART , we could not able to send data ,

Please suggest me any fix the solve the issue?

标签 (3)
0 项奖励
回复
1 回复

690 次查看
June_Lu
NXP TechSupport
NXP TechSupport

You could refer to the DTS below:

https://github.com/nxp-imx/linux-imx/blob/lf-6.6.y/arch/arm64/boot/dts/freescale/imx93-11x11-evk-lpu...

Using command:

stty -F /dev/ttyLPx crtscts to turn it on.

And then echo and cat command.

Good reference:

https://community.nxp.com/t5/i-MX-Processors/i-MX6-how-to-use-RTS-CTS-properly-using-UART-DTE-DCE/m-...

0 项奖励
回复