Trusted Platform Module TPM2.0 in iMX8 Security Controller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Trusted Platform Module TPM2.0 in iMX8 Security Controller

8,557 次查看
m_mansour
Contributor I

Is it possible to implement the TPM2.0 (Trusted Platform Module) standard with the security controller in iMX8, or are there TPM functions that need an external TPM chip?

标记 (3)
0 项奖励
回复
4 回复数

7,186 次查看
MartinHollerweger
NXP Employee
NXP Employee

See also how an NXP SE05x can provide TPM like functionality : https://www.nxp.com/docs/en/application-note/AN12663.pdf

 

8,218 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

   I've sent You some comments directly.

Regards,

Yuri.

0 项奖励
回复

8,125 次查看
sebastian_feick
Contributor I

Hi Yuri,

same question here. Could you sent me the comments as well?

Regards, Sebastian

0 项奖励
回复

8,103 次查看
Yuri
NXP Employee
NXP Employee

@sebastian_feick 
Hello,

      "We're not aware of any NXP activities to support directly the TPM specification.
But taking a look at internal Community,  seems, that it is possible to connect the TPM
using the I2C bus (SMBUS can be controlled via 2-wire interface which is basically
similar with I2C - here [1] you have a datasheet explained  that).

[1] http://pdf.dzsc.com/200810212/297705.pdf

"

Regards,
Yuri.

0 项奖励
回复