Trouble with deinterlacing NTCS/PAL video with an IMX8MP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trouble with deinterlacing NTCS/PAL video with an IMX8MP

3,504 Views
amberworth
Contributor III

Deinterlacing does not work on Yocto Linux, based on kernel 5.10.35.

 

We have adv748x connected to i.MX8MP using MIPI-CSI interface.

adv748x receive NTSC signal and transmit it over CSI interface to i.MX8MP.

 

here is output of the media-ctl -p command

Media controller API version 5.10.35

 

Media device information

------------------------

driver          mxc-md

model           FSL Capture Media Device

serial          

bus info        

hw revision     0x0

driver version  5.10.35

 

Device topology

- entity 1: mxc_isi.0 (16 pads, 2 links)

            type V4L2 subdev subtype Unknown flags 0

pad0: Sink

<- "mxc-mipi-csi2.0":4 [ENABLED]

pad1: Sink

pad2: Sink

pad3: Sink

pad4: Sink

pad5: Sink

pad6: Sink

pad7: Sink

pad8: Sink

pad9: Sink

pad10: Sink

pad11: Sink

pad12: Source

-> "mxc_isi.0.capture":0 [ENABLED]

pad13: Source

pad14: Source

pad15: Sink

 

- entity 18: mxc_isi.0.capture (1 pad, 1 link)

             type Node subtype V4L flags 0

             device node name /dev/video3

pad0: Sink

<- "mxc_isi.0":12 [ENABLED]

 

- entity 22: mxc-mipi-csi2.0 (8 pads, 2 links)

             type Node subtype V4L flags 0

             device node name /dev/v4l-subdev0

pad0: Sink

<- "adv748x 2-0070 txa":1 [ENABLED,IMMUTABLE]

pad1: Sink

pad2: Sink

pad3: Sink

pad4: Source

-> "mxc_isi.0":0 [ENABLED]

pad5: Source

pad6: Source

pad7: Source

 

- entity 31: adv748x 2-0070 txa (2 pads, 3 links)

             type V4L2 subdev subtype Unknown flags 0

             device node name /dev/v4l-subdev3

pad0: Sink

[fmt:UYVY8_2X8/720x240 field:alternate colorspace:smpte170m]

<- "adv748x 2-0070 afe":8 [ENABLED]

<- "adv748x 2-0070 hdmi":1 []

pad1: Source

[fmt:UYVY8_2X8/720x240 field:alternate colorspace:smpte170m]

-> "mxc-mipi-csi2.0":0 [ENABLED,IMMUTABLE]

 

- entity 34: adv748x 2-0070 afe (9 pads, 1 link)

             type V4L2 subdev subtype Decoder flags 0

             device node name /dev/v4l-subdev1

pad0: Sink

pad1: Sink

pad2: Sink

pad3: Sink

pad4: Sink

pad5: Sink

pad6: Sink

pad7: Sink

pad8: Source

[fmt:UYVY8_2X8/720x240 field:alternate colorspace:smpte170m]

-> "adv748x 2-0070 txa":0 [ENABLED]

 

I'm able to capture with command
gst-launch-1.0 v4l2src device=/dev/video3 ! video/x-raw,width=720,height=240 ! queue ! kmssink

but this command capture only half of image - frame with only odd or only even lines

(720x240 instead 720x480).
When i try to enable deinterlacing it fails:

# gst-launch-1.0 --gst-debug=v4l2src:5 v4l2src device=/dev/video3 ! video/x-raw,width=720,height=240,interlace-mode=interlaced ! queue ! kmssink

 

Setting pipeline to PAUSED ...

Pipeline is live and does not need PREROLL ...

Pipeline is PREROLLED ...

Setting pipeline to PLAYING ...

0:00:00.745451625   776 0xaaab147314c0 DEBUG                v4l2src gstv4l2src.c:515:gst_v4l2src_negotiate:<v4l2src0> caps of src: video/x-raw(format:Interlaced), format=(string)YUY2, framerate=(fraction)[ 0/1, 2147483647/1 ], width=(int)[ 1, 4096 ], height=(int)[ 1, 8192 ], interlace-mode=(string)alternate; video/x-raw, format=(string)YUY2, framerate=(fraction)[ 0/1, 2147483647/1 ], width=(int)[ 1, 4096 ], height=(int)[ 1, 8192 ], interlace-mode=(string){ progressive, interleaved }; video/x-raw(format:Interlaced), format=(string)YUY2, framerate=(fraction)[ 0/1, 2147483647/1 ], width=(int)[ 1, 4096 ], height=(int)[ 1, 8192 ], interlace-mode=(string)alternate; video/x-raw(format:Interlaced), format=(string)BGRA, framerate=(fraction)[ 0/1, 2147483647/1 ], width=(int)[ 1, 4096 ], height=(int)[ 1, 8192 ], interlace-mode=(string)alternate; video/x-raw, format=(string)BGRA, framerate=(fraction)[ 0/1, 2147483647/1 ], width=(int)[ 1, 4096 ], height=(int)[ 1, 8192 ], interlace-mode=(string){ progressive, interleaved }; video/x-raw(format:Interlaced), format=(string)BGRA, framerate=(fraction)[ 0/1, 2147483647/1 ], width=(int)[ 1, 4096 ], height=(int)[ 1, 8192 ], interlace-mode=(string)alternate; video/x-raw(format:Interlaced), format=(string)BGRx, framerate=(fraction)[ 0/1, 2147483647/1 ], width=(int)[ 1, 4096 ], height=(int)[ 1, 8192 ], interlace-mode=(string)alternate; video/x-raw, format=(string)BGRx, framerate=(fraction)[ 0/1, 2147483647/1 ], width=(int)[ 1, 4096 ], height=(int)[ 1, 8192 ], interlace-mode=(string){ progressive, interleaved }; video/x-raw(format:Interlaced), format=(string)BGRx, framerate=(fraction)[ 0/1, 2147483647/1 ], width=(int)[ 1, 4096 ], height=(int)[ 1, 8192 ], interlace-mode=(string)alternate; video/x-raw(format:Interlaced), format=(string)BGR, framerate=(fraction)[ 0/1, 2147483647/1 ], width=(int)[ 1, 4096 ], height=(int)[ 1, 8192 ], interlace-mode=(string)alternate; video/x-raw, format=(string)BGR, framerate=(fraction)[ 0/1, 2147483647/1 ], width=(int)[ 1, 4096 ], height=(int)[ 1, 8192 ], interlace-mode=(string){ progressive, interleaved }; video/x-raw(format:Interlaced), format=(string)BGR, framerate=(fraction)[ 0/1, 2147483647/1 ], width=(int)[ 1, 4096 ], height=(int)[ 1, 8192 ], interlace-mode=(string)alternate; video/x-raw(format:Interlaced), format=(string)RGB, framerate=(fraction)[ 0/1, 2147483647/1 ], width=(int)[ 1, 4096 ], height=(int)[ 1, 8192 ], interlace-mode=(string)alternate; video/x-raw, format=(string)RGB, framerate=(fraction)[ 0/1, 2147483647/1 ], width=(int)[ 1, 4096 ], height=(int)[ 1, 8192 ], interlace-mode=(string){ progressive, interleaved }; video/x-raw(format:Interlaced), format=(string)RGB, framerate=(fraction)[ 0/1, 2147483647/1 ], width=(int)[ 1, 4096 ], height=(int)[ 1, 8192 ], interlace-mode=(string)alternate; video/x-raw(format:Interlaced), format=(string)NV12, framerate=(fraction)[ 0/1, 2147483647/1 ], width=(int)[ 1, 4096 ], height=(int)[ 1, 8192 ], interlace-mode=(string)alternate; video/x-raw, format=(string)NV12, framerate=(fraction)[ 0/1, 2147483647/1 ], width=(int)[ 1, 4096 ], height=(int)[ 1, 8192 ], interlace-mode=(string){ progressive, interleaved }; video/x-raw(format:Interlaced), format=(string)NV12, framerate=(fraction)[ 0/1, 2147483647/1 ], width=(int)[ 1, 4096 ], height=(int)[ 1, 8192 ], interlace-mode=(string)alternate; video/x-raw(format:Interlaced), format=(string)RGB16, framerate=(fraction)[ 0/1, 2147483647/1 ], width=(int)[ 1, 4096 ], height=(int)[ 1, 8192 ], interlace-mode=(string)alternate; video/x-raw, format=(string)RGB16, framerate=(fraction)[ 0/1, 2147483647/1 ], width=(int)[ 1, 4096 ], height=(int)[ 1, 8192 ], interlace-mode=(string){ progressive, interleaved }; video/x-raw(format:Interlaced), format=(string)RGB16, framerate=(fraction)[ 0/1, 2147483647/1 ], width=(int)[ 1, 4096 ], height=(int)[ 1, 8192 ], interlace-mode=(string)alternate

New clock: GstSystemClock

0:00:00.745651375   776 0xaaab147314c0 DEBUG                v4l2src gstv4l2src.c:523:gst_v4l2src_negotiate:<v4l2src0> caps of peer: video/x-raw, width=(int)720, height=(int)240, interlace-mode=(string)interlaced, format=(string){ BGRx, BGRA, RGBx, RGBA, NV12_10LE }, framerate=(fraction)[ 0/1, 2147483647/1 ]

0:00:01.078356375   776 0xaaab147314c0 DEBUG                v4l2src gstv4l2src.c:529:gst_v4l2src_negotiate:<v4l2src0> intersect: EMPTY

ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Internal data stream error.

Additional debug info:

../git/libs/gst/base/gstbasesrc.c(3127): gst_base_src_loop (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:

streaming stopped, reason not-negotiated (-4)

Execution ended after 0:00:00.333395500

Setting pipeline to NULL ...

Freeing pipeline ...

 

I investigated the imx8-isi-hw.c and didn't find deinterlacing implementation.
There are 2 functions mxc_isi_channel_deinterlace_init and mxc_isi_channel_set_deinterlace but first of them is empty and second is never used.

 

Maybe I use wrong pipeline?

Is there other way to get interlaced image from the Capture Media Device?
Is there implementation of the ISI deinterlacing?

0 Kudos
Reply
7 Replies

68 Views
petero5
Contributor III

Did anyone ever manage to get odd/even (aka top/bottom) indications from v4l2_buffer via i.MX 8 MIPI CSI-2 (imx8-isi, mxc_isi)?

I'm managing to dequeue interlaced frames (50 fps, 720 x 288) from ADV7280A-M.

But the members of the v4l2_buffer are not changing to indicate odd/even.

https://community.nxp.com/t5/i-MX-Processors/Does-i-MX-8X-support-V4L2-FIELD-ALTERNATE-with-MIPI-CSI...

0 Kudos
Reply

3,176 Views
marioschuknecht
Contributor III

Hi amberworth,

 

Were you able to get deinterlacing NTCS/PAL to work with the mx8mplus?

 

Regards,

Mario

0 Kudos
Reply

3,431 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply

3,128 Views
marioschuknecht
Contributor III

Hi igor

 

So far I have no success to deinterlace frames of the adv7280a-m with the i.MX8MP. Even with the patch applied to kernel 5.4

 

Basically frames can be received via mipi csi-2 on the i.MX8MP. Only as soon as i.MX8MP deinterlacing is activated, nothing happens.

 

Here the register dump for PAL (frame 720x576, field 720x288), Deinterlace method is weaving, no blending, no ntsc_top.

[  130.526648] ISI CHNLC register dump, isi0
[  130.530928]            CHNL_CTRL[0x00]: e0000000
[  130.535661]        CHNL_IMG_CTRL[0x04]: 20002001
[  130.540383]    CHNL_OUT_BUF_CTRL[0x08]: 7c707
[  130.544850]         CHNL_IMG_CFG[0x0c]: 12002d0
[  130.549488]             CHNL_IER[0x10]: 3cfc0000
[  130.554231]             CHNL_STS[0x14]: 100
[  130.558520]    CHNL_SCALE_FACTOR[0x18]: 10001000
[  130.563254]    CHNL_SCALE_OFFSET[0x1c]: 00
[  130.567467]        CHNL_CROP_ULC[0x20]: 00
[  130.571681]        CHNL_CROP_LRC[0x24]: 00
[  130.575884]      CHNL_CSC_COEFF0[0x28]: 00
[  130.580090]      CHNL_CSC_COEFF1[0x2c]: 00
[  130.584291]      CHNL_CSC_COEFF2[0x30]: 00
[  130.588502]      CHNL_CSC_COEFF3[0x34]: 00
[  130.592709]      CHNL_CSC_COEFF4[0x38]: 00
[  130.596920]      CHNL_CSC_COEFF5[0x3c]: 00
[  130.601128]     CHNL_ROI_0_ALPHA[0x40]: 00
[  130.605342]       CHNL_ROI_0_ULC[0x44]: 00
[  130.609555]       CHNL_ROI_0_LRC[0x48]: 00
[  130.613762]     CHNL_ROI_1_ALPHA[0x4c]: 00
[  130.617969]       CHNL_ROI_1_ULC[0x50]: 00
[  130.622180]       CHNL_ROI_1_LRC[0x54]: 00
[  130.626385]     CHNL_ROI_2_ALPHA[0x58]: 00
[  130.630591]       CHNL_ROI_2_ULC[0x5c]: 00
[  130.634800]       CHNL_ROI_2_LRC[0x60]: 00
[  130.639002]     CHNL_ROI_3_ALPHA[0x64]: 00
[  130.643220]       CHNL_ROI_3_ULC[0x68]: 00
[  130.647431]       CHNL_ROI_3_LRC[0x6c]: 00
[  130.651637] CHNL_OUT_BUF1_ADDR_Y[0x70]: 6a400000
[  130.656361] CHNL_OUT_BUF1_ADDR_U[0x74]: 00
[  130.660570] CHNL_OUT_BUF1_ADDR_V[0x78]: 00
[  130.664774]   CHNL_OUT_BUF_PITCH[0x7c]: 5a0
[  130.669069]     CHNL_IN_BUF_ADDR[0x80]: 00
[  130.673277]    CHNL_IN_BUF_PITCH[0x84]: 00
[  130.677480]     CHNL_MEM_RD_CTRL[0x88]: 00
[  130.681688] CHNL_OUT_BUF2_ADDR_Y[0x8c]: 6a100000
[  130.686414] CHNL_OUT_BUF2_ADDR_U[0x90]: 00
[  130.690623] CHNL_OUT_BUF2_ADDR_V[0x94]: 00
[  130.694831]     CHNL_SCL_IMG_CFG[0x98]: 12002d0
[  130.699469]       CHNL_FLOW_CTRL[0x9c]: 00

 Are the registers configured correctly?

Any idea what the problem could be?

 

Thanks in advance.

Mario

 

0 Kudos
Reply

2,876 Views
akochubey
Contributor I

Just in case anyone would be interested:

I had exactly the same problem (IMX8QM): MIPI CSI2 block receives frames OK, but as soon as deinterlace is turned on in ISI, no frames are getting through ISI.

This could be "fixed" by setting VC_INTERLACED (0x30) MIPI CSI CSR register to appropriate value (to me, VC0 is interlaced). I had to modify drivers/staging/media/imx/imx8-mipi-csi2.c to do this.

Frames are getting through after that change.

 

However, the result was ... a bit disappointing. "Need more work".

1. There is 50% chance that ISI weaving deinterlacing will result in a corrupted video.

It seems that odd/even flags are lost somewhere between CSI and ISI and ISI uses wrong field order. As a result, lines order is wrong and instead of getting smooth picture, you get it very "minecraft"-styled.

In CSI protocol, there is "F-bit", which indicates even/odd field, but it is unclear to me how it passes CSI -> Pixel Link -> ISI chain. Ref.Manual says "VC Interlaced - to drive the interlace port of the Pixel Link Master, via the HSYNC/VSYNC generator."

If that is simply counts up VSYNCs, it will never work, of course (right as observed, 50/50). If so, the only working deinterlace method would be blending (?).

2. Color space conversion stopped to work.

I'm unable to tell whether this is intended behaviour, because to my understanding, only "blending" requires CSC resources and weaving only requires different RAM layout at the output block.

Again, documentation is unclear here. See CHNL_BYPASS of ISI CHNL_CTRL CSR in Ref.Manual.

0 Kudos
Reply

2,321 Views
ToarteFretter
Senior Contributor I

Hi,

It seems we have the same problem over here on the i.MX8QM…

Were you able to get the odd/even issue solved?

We’re also wondering how the odd/even is getting transferred over the pixel link between the MIPI-CSI and the ISI? The MIPI signals described in the reference manual do not contain any F-signal too…

We have also 50% chance that the odd/even fields are ordered/deinterlaced in the right way. This for both NTSC and PAL signals arriving (decoded) digitally on the MIPI input.

And if you would be curious, the blending mode has exactly the same problem. The problem is already visible in the intermediate YUYV image generated by ISI channel 1, which then enters ISI channel 0.

Any help or feedback would be nice.

Thanks!

Regards.

0 Kudos
Reply

3,088 Views
marioschuknecht
Contributor III

I was able to find out the following:

 

The interrupt callback mipi_csis_irq_handler of drivers/staging/media/imx/imx8-mipi-csi2-sam.c is executed 50 times per second. And the error bit status is always set to 00001000. The bit 12 means "Indication of lost of Frame Start packet, CH0."

But if deinterlacing is disabled, frames are received and error bit 12 is also set.

Can "lost of Frame Start packet" have influence on deinterlacing?

And without de-interlacing the frames are passed through?

0 Kudos
Reply