Trigger RESETBMCU signal of PF0100 from I2C interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trigger RESETBMCU signal of PF0100 from I2C interface

ソリューションへジャンプ
1,604件の閲覧回数
valterm
Contributor II

We are using i.MX (Solo, DL, dual and quad) with PF0100 PMIC chip.

We would like to trigger the RESETBMCU signal from software, to ensure that hardware reset and SW reset behave in exactly the same way on our device (we use the signal as reset also for additional devices on our board).

Currently we use the internal watchdog to reset the CPU, but this does not tigger the signal on the PMIC.

The PMIC has an I2C interface, but checking the datasheet, I couldn't find a command/register bit that can trigger a reset or re-execute the power-up sequence.

Is it possible to trigger a reset/power-up sequence using the I2C interface?

ラベル(5)
0 件の賞賛
返信
1 解決策
1,421件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately it is not possible to trigger a reset/power-up sequence using I2C interface, what you can do as a possible alternative is to connect a GPIO signal from the processor to the PWRON pin of the PMIC to act as “Reset” signal (typically connected to an external “reset push-button”), and set the following configuration on the PMIC:

PWRON_CFG bit = 1,

SWxOMODE bit = 0,

PWRONRSTEN = 1 and

RESTARTEN = 1

PWRON held low for longer than 4.0 seconds.

This will cause the complete system to restart automatically.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,422件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately it is not possible to trigger a reset/power-up sequence using I2C interface, what you can do as a possible alternative is to connect a GPIO signal from the processor to the PWRON pin of the PMIC to act as “Reset” signal (typically connected to an external “reset push-button”), and set the following configuration on the PMIC:

PWRON_CFG bit = 1,

SWxOMODE bit = 0,

PWRONRSTEN = 1 and

RESTARTEN = 1

PWRON held low for longer than 4.0 seconds.

This will cause the complete system to restart automatically.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信