Touch driver porting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Touch driver porting

2,614件の閲覧回数
chenhungwei
Contributor I

Hello everyone, I have touch driver problem need your help,
I use i.MX6Q with Yocto.
I have changed the new panel, the display is shown normally, but cannot touch(Please see the picture at bottom),
I have checked the DTS & GPIO are normally, the evtest is normally too(reporting the X-Y axis correctly),
I also check the following command and all of them are normally,
could anyone can help me to solve this issue?

A01.png

A02.png

A04.png

A03.png

ラベル(7)
0 件の賞賛
返信
3 返答(返信)

2,512件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Chen

may be useful to check boundary devices touchscreen resources :

https://boundarydevices.com/tag/touch-screen/ 

Sabrelite: New FT5x06 touch screen and swapped Y (input_set_abs_params) 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,512件の閲覧回数
chenhungwei
Contributor I

Hi igorpadykov, 

          Nice to receive your response, do you think this issue is caused by touch driver?

0 件の賞賛
返信

2,512件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

yes I believe it may be caused by driver.

 

Best regards
igor

0 件の賞賛
返信