Too Many CRC and ECC errors on MIPI CSI2 lane of iMX8MMini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Too Many CRC and ECC errors on MIPI CSI2 lane of iMX8MMini

Jump to solution
8,426 Views
efecan_icoz
Contributor III

Hi all,

I'm trying to implement this patch to imx8mm and i've finally made to capture some data over the mipi csi2 bus. But my current issue is; i have a lot CRC and ECC errors while streaming with gstreamer, with command below:

gst-launch-1.0 v4l2src device="/dev/video0" ! "video/x-raw, format=(string)UYVY, width=(int)1280, height=(int)720, framerate=(fraction)25/1" ! videoconvert !  autovideosink‍

And it's stderr output:

Additional debug info:
../../../../git/libs/gst/base/gstbasesink.c(3005): gst_base_sink_is_too_late (): /GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0/GstWaylandSink:autovideosink0-actual-sink-wayland:
There may be a timestamping problem, or this computer is too slow.
WARNING: from element /GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0/GstWaylandSink:autovideosink0-actual-sink-wayland: A lot of buffers are being dropped.
Additional debug info:
../../../../git/libs/gst/base/gstbasesink.c(3005): gst_base_sink_is_too_late (): /GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0/GstWaylandSink:autovideosink0-actual-sink-wayland:
There may be a timestamping problem, or this computer is too slow.
WARNING: from element /GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0/GstWaylandSink:autovideosink0-actual-sink-wayland: A lot of buffers are being dropped.
‍‍‍‍‍‍‍‍

And the capture/error rate from csi driver's debug log of 16 second stream:

[  239.518263] mxc_mipi-csi.0: mipi_csis_s_stream: 0, state: 0x3
[  239.518277] mxc_mipi-csi.0: Frame End events: 166
[  239.522981] mxc_mipi-csi.0: Frame Start events: 158
[  239.527859] mxc_mipi-csi.0: Non-image data after odd frame events: 0
[  239.534211] mxc_mipi-csi.0: Non-image data before odd frame events: 0
[  239.540649] mxc_mipi-csi.0: Non-image data after even frame events: 0
[  239.547086] mxc_mipi-csi.0: Non-image data before even frame events: 0
[  239.553611] mxc_mipi-csi.0: Unknown Error events: 0
[  239.558485] mxc_mipi-csi.0: CRC Error events: 264610
[  239.563447] mxc_mipi-csi.0: ECC Error events: 426
[  239.568148] mxc_mipi-csi.0: FIFO Overflow Error events: 0
[  239.573544] mxc_mipi-csi.0: Lost Frame End Error events: 13
[  239.579113] mxc_mipi-csi.0: Lost Frame Start Error events: 148505
[  239.585203] mxc_mipi-csi.0: SOT Error events: 0
‍‍‍‍‍‍‍‍‍‍‍‍‍‍

I'm using MIPI CSI2 in 4 lane 1 channel mode in YUV422 format.

I just cant understand why the CRC & ECC errors happen and i can't debug/analyse deeper this situation. But i have some questions that is unanswered.

1) What is the use of hs-settle and clk-settle ? Reference manual doesn't have any info about those fields of MIPI registers. I can only find out this post but since imx8mm is differs way too many aspects from other platforms I'm not sure if that applies to my board too.

2) Why csi driver uses MEDIA_BUS_FMT_YUYV8_2X8 format as media format of YUV422 instead of MEDIA_BUS_FMT_UYVY8_2X8 ? Isn't bus format of YUV422 standard as UYVY as stated in MIPI standart or am i comparing apples and oranges in here can someone explain that ?

Labels (1)
0 Kudos
Reply
1 Solution
8,176 Views
efecan_icoz
Contributor III

TL; DR; solution is D2P lane of mipi csi bus is shorted to GND this was creating the error.

If anyone faces this problem, first of all check your connections continuity. If you have a scope or signal analyzer check every line to see if they are alive.

View solution in original post

0 Kudos
Reply
4 Replies
8,177 Views
efecan_icoz
Contributor III

TL; DR; solution is D2P lane of mipi csi bus is shorted to GND this was creating the error.

If anyone faces this problem, first of all check your connections continuity. If you have a scope or signal analyzer check every line to see if they are alive.

0 Kudos
Reply
8,176 Views
igorpadykov
NXP Employee
NXP Employee

Hi Efe

thanks for sharing solution. Camera can be tested using

MINISASTOCSI daughter card and fsl-imx8mm-evk.dtb :

$ gst-launch1.0 v4l2src device=/dev/video0 ! autovideosink

Yes, for hs-settle and clk-settle one can use this post since imx8mm 

has the same IP.

Best regards
igor

0 Kudos
Reply
8,176 Views
efecan_icoz
Contributor III

Hi Igor,

Do you have any idea about my second question ?

Have a nice day,
Efe

0 Kudos
Reply
8,176 Views
igorpadykov
NXP Employee
NXP Employee

Hi Efe

strictly speaking this patch is for another processor - i.MX8QM

which is quite different from i.MX8M Mini.

Suggest to look at native i.MX8M Mini driver described in

Linux 5.4.3_1.0.0 Documentation and create new thread.

Best regards
igor

0 Kudos
Reply