To effect secure boot immediately, which boot sequence does it need?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

To effect secure boot immediately, which boot sequence does it need?

Jump to solution
5,236 Views
takayuki_ishii
Contributor V

Hello community

In Document "i.MX_6_Linux_High_Assurance_Boot_(HAB)_Users_Guide_201405.pdf",

It have a sequence to put SEC_CONFIG to close in section 4 "Test Procedure".

After write eFuse by echo command,

In chapter 19, it say that "Boot the board again,",

Is this mean that to effect the chip security immediately, it must need a power on/off cycle?

Or it need only reset (POR_B Low cycle) to do that?

To reduce the eFuse write cycle time, customer plan to use "POR_B" cycle for it.

Best regards,

Ishii.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,632 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

you are right, to effect the chip security immediately it is

sufficient only reset (POR_B Low cycle) to do that.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,632 Views
takayuki_ishii
Contributor V

Hello Igor,

Thank you for your quick response.

I will answer it to my customer.

Best regards,

Ishii.

0 Kudos
Reply
1,633 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

you are right, to effect the chip security immediately it is

sufficient only reset (POR_B Low cycle) to do that.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply