Timing of MMPF0100 OTP programming interface.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Timing of MMPF0100 OTP programming interface.

跳至解决方案
1,361 次查看
satoshishimoda
Senior Contributor I

Hi community,

I have a MMPF0100 OTP programming interface.

I understood how to desing the programming interface with AN4536.

However, I have not understood whether there is a timing restrict about the programming interface.

I guess, the AC spec of I2C is compliant to NXP I2C specification, then is there other timing spec between each signals of programming interface?

Best Regards,

Satoshi Shimoda

标记 (3)
0 项奖励
回复
1 解答
1,225 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

there are no other additional special timing requirements

except procedure given in AN4536

AN4536, MMPF0100 OTP Programming Instructions - Application Note.

Also you are right: AC spec of I2C is compliant to NXP I2C specification.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,226 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

there are no other additional special timing requirements

except procedure given in AN4536

AN4536, MMPF0100 OTP Programming Instructions - Application Note.

Also you are right: AC spec of I2C is compliant to NXP I2C specification.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复