Timing of MMPF0100 OTP programming interface.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Timing of MMPF0100 OTP programming interface.

Jump to solution
1,362 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a MMPF0100 OTP programming interface.

I understood how to desing the programming interface with AN4536.

However, I have not understood whether there is a timing restrict about the programming interface.

I guess, the AC spec of I2C is compliant to NXP I2C specification, then is there other timing spec between each signals of programming interface?

Best Regards,

Satoshi Shimoda

Tags (3)
0 Kudos
Reply
1 Solution
1,226 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

there are no other additional special timing requirements

except procedure given in AN4536

AN4536, MMPF0100 OTP Programming Instructions - Application Note.

Also you are right: AC spec of I2C is compliant to NXP I2C specification.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,227 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

there are no other additional special timing requirements

except procedure given in AN4536

AN4536, MMPF0100 OTP Programming Instructions - Application Note.

Also you are right: AC spec of I2C is compliant to NXP I2C specification.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply