Three camera inputs for i.MX6Quad

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Three camera inputs for i.MX6Quad

跳至解决方案
1,382 次查看
yuuki
Senior Contributor II

Dear all,

We would like to connect three cameras to i.MX6.
(CSI Parallel port 2ch + MIPI-CSI port 1ch)

According to i.MX 6 Series Firmware Guide, MIPI and parallel seem to be exclusive.

i.MX 6 Series Firmware Guide Rev.0:
- 21.5 IOMUX pin mapping
- Table 21-4. Camera interface mode setting

Can three ports be inputted simultaneously?
If so, Could you teach the value of Bit19-20 of IOMUXC_GPR1 register which should be set up?

Best Regards,
Yuuki

标签 (1)
1 解答
1,119 次查看
Yuri
NXP Employee
NXP Employee

It is possible to connect three cams to i.MX6.

You may look at Figure 19-1 (CSI2IPU gasket connectivity) of the i.MX6 DQ Reference Manual.

MIPI_CSI.jpg


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,120 次查看
Yuri
NXP Employee
NXP Employee

It is possible to connect three cams to i.MX6.

You may look at Figure 19-1 (CSI2IPU gasket connectivity) of the i.MX6 DQ Reference Manual.

MIPI_CSI.jpg


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复