Three camera inputs for i.MX6Quad

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Three camera inputs for i.MX6Quad

Jump to solution
2,006 Views
yuuki
Senior Contributor I

Dear all,

We would like to connect three cameras to i.MX6.
(CSI Parallel port 2ch + MIPI-CSI port 1ch)

According to i.MX 6 Series Firmware Guide, MIPI and parallel seem to be exclusive.

i.MX 6 Series Firmware Guide Rev.0:
- 21.5 IOMUX pin mapping
- Table 21-4. Camera interface mode setting

Can three ports be inputted simultaneously?
If so, Could you teach the value of Bit19-20 of IOMUXC_GPR1 register which should be set up?

Best Regards,
Yuuki

Labels (1)
Tags (5)
1 Solution
1,743 Views
Yuri
NXP Employee
NXP Employee

It is possible to connect three cams to i.MX6.

You may look at Figure 19-1 (CSI2IPU gasket connectivity) of the i.MX6 DQ Reference Manual.

MIPI_CSI.jpg


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,744 Views
Yuri
NXP Employee
NXP Employee

It is possible to connect three cams to i.MX6.

You may look at Figure 19-1 (CSI2IPU gasket connectivity) of the i.MX6 DQ Reference Manual.

MIPI_CSI.jpg


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply