Thermal protect before execute the uBoot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Thermal protect before execute the uBoot

Jump to solution
2,139 Views
tomo
Contributor II

Dear all

The uboot was not executed in my custom board with MX6 solo when ambient is 90 degrees.
I think it may be thermal protection, does ROM cord check die temperature before execute the uboot?

If so, what is the shutdown temperature?

best regards,

tomo

0 Kudos
Reply
1 Solution
2,070 Views
Yuri
NXP Employee
NXP Employee

Hello,

  i.MX6S boot ROM does not control device temperature.

Regards,

Yuri.

View solution in original post

0 Kudos
Reply
2 Replies
2,071 Views
Yuri
NXP Employee
NXP Employee

Hello,

  i.MX6S boot ROM does not control device temperature.

Regards,

Yuri.

0 Kudos
Reply
2,070 Views
tomo
Contributor II

Thank you for your answer quickly.

Best regards,

tomo

0 Kudos
Reply