The problem of VBR value variation range being too large during imx8mm VPU H264 encoding

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The problem of VBR value variation range being too large during imx8mm VPU H264 encoding

844 次查看
pyh0603
Contributor III

Hi,all

 we are using imx8mm for H264 encoding, system information is as bellow:
    CPU: MIMX8MM6DVTLZAA
    software version: imx-4.14.98-2.0.0_ga.xml
    vpu:====== VPUENC: 4.4.5 build on Oct 30 2019 12:04:50. ====== 
           wrapper: 3.0.0 (VPUWRAPPER_ARM64_LINUX Build on Sep 24 2021 08:24:44)    vpulib: 1.1.1  firmware: 1.1.1.65535
  
    Issues describe:
    If we use the CBR mode, The output bit rate fluctuates by approximately 20%.
    but in the VBR mode, The output bit rate fluctuates about 30k~30M (1080p/60fps, H264 encoding);
   
    however, we test another solution,  its  output bit rate fluctuates  about 30k~5M (most time is 4M);
    so our quetsion is: is it possible to optimize  MIMX8MM vpu for its VBR mode?  can we make it's output bit rate fluctuates from 30k~30M to 30k~5M in VBR mode(1080p/60fps, H264 encoding)? anyother update? or give us some suggetion, thanks.

Looking forward to your reply

0 项奖励
回复
2 回复数

362 次查看
DR_Akzhol
Contributor III

Hello there, could you find a solution for that? We have tested VBR with highprofile mode. At DAY we have normal Bitrate 100kb-3Mb, night time camera gives more noise, so the bitrate goes to 15-20Mb (too big files at night)

0 项奖励
回复

827 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Thanks depend of the video, but with current codecs is not possible to optimize the VBR but there is a VPU manual on your yocto documentation where your can apply the api and check is there optimization.

 

Regards

0 项奖励
回复