The parted command is not executed on Android.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The parted command is not executed on Android.

1,202 Views
DaengCheong
Contributor II

I'm in an environment where I can't use MFGTOOL right now, so I'm trying to boot Android with an SD card and write Android images from Android to eMMC. So I'm trying to import a Linux shell script into Android and run it. I couldn't use the sfdisk, so I tried to use parted, but I couldn't find the parted command, so I asked a question.

I wonder how I can use the parted command. Or is there a way to write Android images to eMMC because MFGTOOL is not available?

Labels (2)
0 Kudos
Reply
1 Reply

1,180 Views
jimmychan
NXP TechSupport
NXP TechSupport

You better to build the Linux BSP with "bitbake core-image-full-cmdline ". For details about howto build the Linux BSP, please refer to the Yocto Guide. (i.MX Yocto Project User’s Guide​)

 

Then, boot Linux with the SD card and then you could write the Android images to EMMC by linux commands. 

0 Kudos
Reply