The minimum pulse width specification for WDOG_B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The minimum pulse width specification for WDOG_B

Jump to solution
2,567 Views
george
Senior Contributor II

Hi all,

  • Does WDOGx_B shown in the i.MX8M-Mini data sheet mean the WDOG_B external output signal?

pastedImage_4.png

  • Or does it mean the wdog_rst internal signal shown in the reference manual?

pastedImage_5.png

We want to know the low width of the WDOG_B external output signal for our product design.

BR,

George

0 Kudos
Reply
1 Solution
2,507 Views
Yuri
NXP Employee
NXP Employee

The external WDOG output signal  (similar as WDOG-1 on the picture)

is not controlled in software.

~Yuri.  

View solution in original post

0 Kudos
Reply
4 Replies
2,507 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The CC3 parameters relates to external output signal:

"WDOGx_B output signals (for each one of the Watchdog modules) do not
have dedicated pins, but are muxed out through the IOMUX"


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,507 Views
george
Senior Contributor II

Dear Yuri,

Thank you for your reply.

  • Does CC3 parameter for external output signal you say mean red mark in the figure below

pastedImage_2.png

  • Can I make the low pulse width longer by Watchdog register settings?
  • Or is this length uncontollable by the user?

BR,

George

0 Kudos
Reply
2,508 Views
Yuri
NXP Employee
NXP Employee

The external WDOG output signal  (similar as WDOG-1 on the picture)

is not controlled in software.

~Yuri.  

0 Kudos
Reply
2,507 Views
george
Senior Contributor II

Thanks.

0 Kudos
Reply