The IMX8's HDMI interface forces the output to a resolution of 4032x756
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I have an 4032x756 lcd I am looking to configure for the imx8m to run it.I am running u-boot 2019.04 and Linux kernel L4.19.35.
My question is how do you generate the required clock speed for a 4032x756&57Hz hdmi LCD?
Here are the screen parameters I use.
I have made the following changes at this time.
I refered to this Driving a 1080x1920 portrait HDMI screen solution.
- add below drm mode in drivers/gpu/drm/imx/hdp/imx-hdp.c
{ DRM_MODE("4032x756", DRM_MODE_TYPE_DRIVER, 148500, 4032, 4110,
4132, 4194, 0, 756, 762, 768, 774, 0,
DRM_MODE_FLAG_PHSYNC | DRM_MODE_FLAG_PVSYNC),
.vrefresh = 50, .picture_aspect_ratio = HDMI_PICTURE_ASPECT_16_9, },
2.I refered to thisCustom Resolution 800x480 - NXP Communitysolution.I find the 《HDMI-pixel clock calculation》,but I do not know how to use it.How to fill in each parameter.
The challenge I am having is what I need to add the spreadsheet for the input variables:
- Reference Clock Freq
- Expected Pixel clock
- Generated clock tolerance
- pll input divider
- pll feedback divider
- pixel clock divider
- character clock divider
Based on the above modeline should I be able to dervice these values or I need more information?
Any guidance is appreciated.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
HI
Is there any technical support, IMX8MM supports more resolutions and clocks? What manual should I refer to? thank

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
The i.MX8M support up to 4Kp60 resolution on the HDMI and 1080p60 on the MIPI-DSI.
For the PLL configuration you may refer to the i.MX8M reference manual chapter 5.1.5.4.4 SSCG and Fractional PLLs
Best regards,
Aldo.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The i.MX8M support up to 4Kp60 resolution on the HDMI and 1080p60 on the MIPI-DSI.
如果同时使用两个HDMI+mipi_dsi,分辨率能够达到多少呢?
1080p+720p是极限么?