The 8mp falcon mode cannot function correctly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The 8mp falcon mode cannot function correctly

769件の閲覧回数
Eddy1
Contributor V

Recently, according to the AN13709.pdf manual, I set up the 8mp falcon feature, but after booting to the kernel, it keeps printing “GICv3: CPU2: ICC_SGI1R_EL1 1000001”. Could you please provide some suggestions?The current version :NXP i.MX Release Distro 5.10-gatesgarth

[ 13.171155] GICv3: CPU2: ICC_SGI1R_EL1 1000001
[ 13.175641] kobject: '30380000.clock-controller--30890000.serial' ((____ptrval____)): kobject_cleanup, parent 0000000000000000
[ 13.187054] kobject: '30380000.clock-controller--30890000.serial' ((____ptrval____)): calling ktype release
[ 13.196878] kobject: '30380000.clock-controller--30890000.serial': free name
[ 13.203960] imx-uart 30890000.serial: Dropping the link to 30330000.pinctrl
[ 13.210941] GICv3: CPU2: ICC_SGI1R_EL1 1000001
[ 13.215440] GICv3: CPU2: ICC_SGI1R_EL1 1000001
[ 13.219908] GICv3: CPU2: ICC_SGI1R_EL1 1000001
[ 13.224369] GICv3: CPU2: ICC_SGI1R_EL1 1000001
[ 13.228830] GICv3: CPU2: ICC_SGI1R_EL1 1000001
[ 13.233291] GICv3: CPU2: ICC_SGI1R_EL1 1000001
[ 13.237755] GICv3: CPU2: ICC_SGI1R_EL1 1000001
[ 13.242220] GICv3: CPU2: ICC_SGI1R_EL1 1000001
[ 13.246684] GICv3: CPU2: ICC_SGI1R_EL1 1000001
[ 13.251149] GICv3: CPU2: ICC_SGI1R_EL1 1000001

 

 

[ 22.966677] mmc0: sdhci-esdhc-imx: fifo debug status: 0x3680
[ 22.972421] mmc0: sdhci-esdhc-imx: async fifo debug status: 0x3750
[ 22.978686] mmc0: sdhci: ============================================
[ 23.351428] rcu: INFO: rcu_preempt detected stalls on CPUs/tasks:
[ 23.357527] rcu: 0-...0: (1 GPs behind) idle=652/1/0x4000000000000000 softirq=80/81 fqs=2621
[ 23.366136] (detected by 2, t=5252 jiffies, g=-975, q=17)

0 件の賞賛
返信
0 返答(返信)