Test tools for android

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Test tools for android

1,818件の閲覧回数
ashokp
Contributor I

Hi All,

I am new to android. I am using IMX6Q based custom board. I need to test all the interfaces in the IMX6 like i2c, SPI, USB, memory, EMMC etc. Is there any tools available in android. Please let me know if any document which describes to test the IMX6 interfaces

Thanks,

P.Ashok

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,421件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ashok,

Android has not dedicated for each module tests.

You should test board modules without operating system (bare-metal)

tests, use SDK

i.MX 6Series Platform SDK

Also test memory with tests below

https://community.freescale.com/message/331721#331721

https://community.freescale.com/docs/DOC-96412

Only when memory and modules were tested it is

recommended to run Android.

Also it is useful to check Android docs, Android_Frequently_Asked_Questions.pdf

IMX6_KK442_100_ANDROID_DOCS

i.MX_6Dual6Quad_BSP_Porting_Guide.pdf in

L3.0.35_4.1.0_LINUX_DOCS

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信