Test tools for android

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Test tools for android

1,817 Views
ashokp
Contributor I

Hi All,

I am new to android. I am using IMX6Q based custom board. I need to test all the interfaces in the IMX6 like i2c, SPI, USB, memory, EMMC etc. Is there any tools available in android. Please let me know if any document which describes to test the IMX6 interfaces

Thanks,

P.Ashok

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,420 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ashok,

Android has not dedicated for each module tests.

You should test board modules without operating system (bare-metal)

tests, use SDK

i.MX 6Series Platform SDK

Also test memory with tests below

https://community.freescale.com/message/331721#331721

https://community.freescale.com/docs/DOC-96412

Only when memory and modules were tested it is

recommended to run Android.

Also it is useful to check Android docs, Android_Frequently_Asked_Questions.pdf

IMX6_KK442_100_ANDROID_DOCS

i.MX_6Dual6Quad_BSP_Porting_Guide.pdf in

L3.0.35_4.1.0_LINUX_DOCS

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply