Test application using IMX6 vpu decoder API's?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Test application using IMX6 vpu decoder API's?

ソリューションへジャンプ
3,917件の閲覧回数
anishkhanna
Contributor I

Hi All,

I have gone through decoding API's provided in the document i.MX 6Dual/6Quad VPU Application Programming Interface Linux Reference Manual.

Can any one please provide a Test application which uses specifically decoder API's. Any help is highly accepted.

Thanks,

Anish.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,715件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

I think you can refer to the V4L2 driver. Please read the i.MX_6Dual6Quad_Linux_Reference_Manual.pdf Chapter 8 for the details.  There is an i.MX Test package in Linux BSP. the package name "imx-test". You can take it as reference.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,716件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

I think you can refer to the V4L2 driver. Please read the i.MX_6Dual6Quad_Linux_Reference_Manual.pdf Chapter 8 for the details.  There is an i.MX Test package in Linux BSP. the package name "imx-test". You can take it as reference.

0 件の賞賛
返信
2,715件の閲覧回数
johnturnur
Contributor III

Hi

Jimmy

Can this test works on Android platform?

And what are the step to perform this step.


0 件の賞賛
返信
2,715件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

I didn't try it on Android. Seems someone can use it in Android. Maybe you can read this post for reference.

https://community.freescale.com/message/286492#286492

0 件の賞賛
返信