Test application using IMX6 vpu decoder API's?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Test application using IMX6 vpu decoder API's?

Jump to solution
3,908 Views
anishkhanna
Contributor I

Hi All,

I have gone through decoding API's provided in the document i.MX 6Dual/6Quad VPU Application Programming Interface Linux Reference Manual.

Can any one please provide a Test application which uses specifically decoder API's. Any help is highly accepted.

Thanks,

Anish.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,706 Views
jimmychan
NXP TechSupport
NXP TechSupport

I think you can refer to the V4L2 driver. Please read the i.MX_6Dual6Quad_Linux_Reference_Manual.pdf Chapter 8 for the details.  There is an i.MX Test package in Linux BSP. the package name "imx-test". You can take it as reference.

View solution in original post

0 Kudos
Reply
3 Replies
2,707 Views
jimmychan
NXP TechSupport
NXP TechSupport

I think you can refer to the V4L2 driver. Please read the i.MX_6Dual6Quad_Linux_Reference_Manual.pdf Chapter 8 for the details.  There is an i.MX Test package in Linux BSP. the package name "imx-test". You can take it as reference.

0 Kudos
Reply
2,706 Views
johnturnur
Contributor III

Hi

Jimmy

Can this test works on Android platform?

And what are the step to perform this step.


0 Kudos
Reply
2,706 Views
jimmychan
NXP TechSupport
NXP TechSupport

I didn't try it on Android. Seems someone can use it in Android. Maybe you can read this post for reference.

https://community.freescale.com/message/286492#286492

0 Kudos
Reply