Termination resistor value

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Termination resistor value

1,403 Views
johnnynguyen
Contributor I

I am connecting a i.MX6UL processor Ethernet interface to a FPGA through RMII, and the FPGA is converting to 1G Ethernet to the switch. So between the processor and FPGA, the transmission lines have to be terminated. What is the source resistance of the processor? what type and value resistor I should use to terminate the reflection?

Thanks

Labels (1)
0 Kudos
Reply
1 Reply

1,279 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nguyen

please check sect.3.8 Impedance signal recommendations i.MX6UL System Development User’s Guide

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6ULHDG.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply