Termination resistor value

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Termination resistor value

1,406件の閲覧回数
johnnynguyen
Contributor I

I am connecting a i.MX6UL processor Ethernet interface to a FPGA through RMII, and the FPGA is converting to 1G Ethernet to the switch. So between the processor and FPGA, the transmission lines have to be terminated. What is the source resistance of the processor? what type and value resistor I should use to terminate the reflection?

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

1,282件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nguyen

please check sect.3.8 Impedance signal recommendations i.MX6UL System Development User’s Guide

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6ULHDG.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信