Termination resistor value

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Termination resistor value

1,404 次查看
johnnynguyen
Contributor I

I am connecting a i.MX6UL processor Ethernet interface to a FPGA through RMII, and the FPGA is converting to 1G Ethernet to the switch. So between the processor and FPGA, the transmission lines have to be terminated. What is the source resistance of the processor? what type and value resistor I should use to terminate the reflection?

Thanks

标签 (1)
0 项奖励
回复
1 回复

1,280 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nguyen

please check sect.3.8 Impedance signal recommendations i.MX6UL System Development User’s Guide

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6ULHDG.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复