Tensorflow Lite 2.2.0 NNAPI memory reak in L5.4.47_2.2.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Tensorflow Lite 2.2.0 NNAPI memory reak in L5.4.47_2.2.0

2,654 次查看
hsaito
Contributor I

Operating environment is i.mx8qm, using L5.4.47_2.2.0.

We modified label_image.py to check the operation of sensorflow Lite 2.2.0, which uses NNAPI.

The fix is to call Invoke() process continuously.(I have pasted the modified program label_image.py.)

My goal is to use camera footage to perform inference processing, but will using NNAPI cause memory leaks?

Is there any way to improve it?

The starting memory usage is shown in before.png and the memory usage after about an hour is shown in after.png.

 

0 项奖励
回复
2 回复数

2,627 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using NXP i.MX8QM reference board?

0 项奖励
回复

2,626 次查看
hsaito
Contributor I

This result is our original board.

However, the memory usage continues to increase even when I run it on the evaluation board.

0 项奖励
回复