Tensorflow Lite 2.2.0 NNAPI memory reak in L5.4.47_2.2.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Tensorflow Lite 2.2.0 NNAPI memory reak in L5.4.47_2.2.0

2,659件の閲覧回数
hsaito
Contributor I

Operating environment is i.mx8qm, using L5.4.47_2.2.0.

We modified label_image.py to check the operation of sensorflow Lite 2.2.0, which uses NNAPI.

The fix is to call Invoke() process continuously.(I have pasted the modified program label_image.py.)

My goal is to use camera footage to perform inference processing, but will using NNAPI cause memory leaks?

Is there any way to improve it?

The starting memory usage is shown in before.png and the memory usage after about an hour is shown in after.png.

 

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,632件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using NXP i.MX8QM reference board?

0 件の賞賛
返信

2,631件の閲覧回数
hsaito
Contributor I

This result is our original board.

However, the memory usage continues to increase even when I run it on the evaluation board.

0 件の賞賛
返信