Tensorflow Lite 2.2.0 NNAPI memory reak in L5.4.47_2.2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Tensorflow Lite 2.2.0 NNAPI memory reak in L5.4.47_2.2.0

2,591 Views
hsaito
Contributor I

Operating environment is i.mx8qm, using L5.4.47_2.2.0.

We modified label_image.py to check the operation of sensorflow Lite 2.2.0, which uses NNAPI.

The fix is to call Invoke() process continuously.(I have pasted the modified program label_image.py.)

My goal is to use camera footage to perform inference processing, but will using NNAPI cause memory leaks?

Is there any way to improve it?

The starting memory usage is shown in before.png and the memory usage after about an hour is shown in after.png.

 

0 Kudos
Reply
2 Replies

2,564 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using NXP i.MX8QM reference board?

0 Kudos
Reply

2,563 Views
hsaito
Contributor I

This result is our original board.

However, the memory usage continues to increase even when I run it on the evaluation board.

0 Kudos
Reply