Temperature sensor connectivity

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Temperature sensor connectivity

5,343件の閲覧回数
logeshs
Contributor II

Hi,

We are using IMXD7 application processor (MCIMX7D3EVK10SD ) for our wearable design.  When exploring the options for connecting external temperature sensors with the processor, we found from the datasheet that  we have a pin named TEMPSENSOR_REXT. This pin is recommended to connect to a 100k resistor to ground. Our query is that can we use this pin for external thermistor connection. Can the internal temperature sensor monitor module use this pin for temperature sensing. If yes please provide required inputs for the same.

 

Is there any other recommended way to connect external thermistors to IMX7D processor.

Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,433件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Logesh

EMPSENSOR_REXT is used for biasing internal temperature sensor,

it can not be used for external thermistors. External thermistors can be

connected to adc (with additional precision resistor connected to stable

reference voltage source).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信