Temperature dependent on DDR memory calibration ? Reason for kernel panic when the imx6q system get heat-up ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Temperature dependent on DDR memory calibration ? Reason for kernel panic when the imx6q system get heat-up ?

2,341 Views
peteramond
Contributor V

Hi All,

I have done DDR memory calibration for my imx6q custom hardware design in ambient temperature and got proper and reliable read,write,dqs gating values for DDR memory. And I updated u-boot configs according to those values. 

But when the system get heat up; as an example when the die temperature of the imx6 exceed 55C the system shows kernel panic. It is difficult to identify the reason using the errors pop-up in kernel panic using program counter. (May be this is not a reason in processor because imx6 can work up to 85C without de-clocking) 

  1. Do we need to do DDR memory calibration in different temperatures before do the updates in u-boot ? Any dependency on memory calibration on temperature ?
  2. How can we get temperature profile using few thermocouples which were placed on different areas of DDR memory chips, imx6 processor and etc by using imx6q libraries ?

Regards,

Peter.

Labels (3)
2 Replies

1,856 Views
igorpadykov
NXP Employee
NXP Employee

Hi Peter

1. if heating up the part causes more failures, then the drive strength is too low and the
signals may not rise/fall fast enough. There is no need to perform DDR memory calibration in
different temperatures, temperature influence is described in sect.7.2 ZQ Calibration Usage
AN4467 i.MX6 Series DDR Calibration
http://cache.nxp.com/docs/en/application-note/AN4467.pdf
2. please refer to AN4579 i.MX 6 Series Thermal Management Guidelines
http://cache.nxp.com/docs/en/application-note/AN4579.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,856 Views
peteramond
Contributor V

Hi igor,

@igorpadykov

Thank you for your explanation. 

Today I encountered a new problem with my iMX6Q custom hardware design with Linux version 4.1.15-1.0.0_ga+yocto+g76c24a0

I have an issue with GPU during I launch cameras (System stuck).

Camera launch >> gst-launch-1.0 v4l2src device=/dev/video0 ! autovideosink

Error message >> [galcore]: GPU[0] hang, automatic recovery.

It shows the test patterns without any conflict. When I run

gst-launch-1.0 videotestsrc pattern=0 ! autovideosink

There are no any conflict.

What can be the cause of this issue ?

Regards,

Peter.

0 Kudos
Reply