TV In Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TV In Issue

1,736件の閲覧回数
madstrum
Contributor III

I'm trying to get Tv In from a analog output camera.

Using Gstreamer, I did

gst-launch-0.10 tvsrc ! autovideosink

I got tvsrc from these forums.

It gives me this error :

MFW_GST_tvsrc_PLUGIN 3.0.7 build on ....

Setting pipeline to paused ...

MFW_GST_V4LSINK_PLUGIN 3.0.7 .....

ERROR : Pipeline doesn't want to pause.

Setting pipeline to BULL ...

Total rendered:0

[----> FINALIZE v4l_sink

Freeing pipeline

How do I resolve this? Has anyone done something similar?

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,612件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

We are reviewing your request internally, you will get an update soon. 

Best regards!

/Carlos

0 件の賞賛
返信

1,612件の閲覧回数
madstrum
Contributor III

It's ok it was a hardware fault on the baseboard.

0 件の賞賛
返信