I was wondering if anyone knows where I can find DISP0_DATxx single-ended output impedance information for the i.mx6?
I've looked in the i.mx6 Techinical Datasheet (IMX6DQAEC.pdf) under 'Electrical Characteristics'->'Image Processing Unit (IPU)' and found nothing.
The other peripherals 'LVDS' and 'MIPI D-PHY' both contain the 'Singled-Ended Output Impedance' information, but the display port's cannot be located.
Any help would be greatly appreciated.
Thanks.
Hi K R
for these pins please use
sect.4.8.1 GPIO Output Buffer Impedance IMX6DQCEC
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Igor,
It seems upon verifying this in software under the register:
IOMUXC_SW_PAD_CTL_PAD_DISP0_DATA00
found in: IMX6DQRM
We get a value of '000' for the DSE (drive strength field). Can I assume that this is the correct register and field?
Also, we are outputting data on this pin, but still have a value of high impedance for the drive strength. Is this normal?
Thanks.
Kyle
Hi K R
yes DSE is correct setting for impedance.
You can check with other pads and configure as GPIO
just for test.
Best regards
igor